This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: Asking for the BQ25703A schematic review

Part Number: BQ25703A

Hi Team,

Customer would like to use BQ25703A.

Here is the design spec.

Input source:

  1. DC Jack: 12V/2.5A
  2. PD:5V/3A, 9V/3A
  3. QC:9V/1.67A
  4. Wall charger: 5V/1.5A

 

  • Charging voltage: 8.8V
  • Charging Current: 3A

 

 

Attached file is BQ25703A schematic and register setting.

 

 Please provide view the schematic and provide your comment.

 BR,

SHH