Tool/software: Code Composer Studio
1,Application is like that board with battery is in system for 5 years. Battery will charge to 4.2V(100%). Then there is an leakage current 10mA to discharge battery to 95%(4.1V) with 2days. And battery will charge it again to full. Discharge current threshold is 100mA. My problem is how to know battery real capacity (or SOH) during this period? Can unfiltered RM, unfiltered FCC and truesoc indicate real capacity of battery?
2, If Battery will charge to 4.2V(100%). Then there is an leakage current 10mA to discharge battery to low soc. Can this process update Ra table and Qmax?
3,Because our leakage current is about 10mA. If I set dsg current threshold below to 10mA, can Ra table and Qmax update and be accurate?
4,As SLUA450 states 'In order to ensure high accuracy of the DOD measurement, the Qmax calculation does not occur if the temperature is above 40°C, or below 10°C.' But in our application, battery temp is about 60C normally. Could you modify temperature threshold allowed to update Qmax? How? This temperature is the reading 'temperature parameter' of FG, is it right? (cell is INR18650A from Moli)
5, As you said 'if you have completed your golden learning cycle, then you need just 37% of design capacity passed charge for qmax to update.' Could I modify threshold of 37% to 5% for Qmax update? Will it be accurate?
6,There are two groups of Ra table and Qmax 0 and 1. Once FG choose group 0 for battery at the beginning. Is it possible for this battery to change to use group 1 during its 5 service years?
7,Even if I can update Ra during service time, it just updates 'Ra0 table' and other 5 tables are same with original data. So I think it is useless for RM,FCC's accuracy. Because FG may still use Ra table that didn't update. Is it right?
8,Do Ra0, Ra0x and Ra0 default tables(or Ra1, Ra1x and Ra1 default tables ) update during discharge when this FW completed learning cycle? How do you make sure FG still use updated Ra instead of Ra without update?
9,What method does FG use to choose which Ra table to use?
10,Please according to your experience and calculation method, tell me a deviation between unfiltered RM and actual unfiltered RM after 2 years(2 times of original impedance)?
Thanks!