Other Parts Discussed in Thread: TPS61194
Hi sir,
my customer is using TPS61194-Q1 for a 4s13p panel's backlight , but when the board power on , the screen will flicker and the inductor will happen Whistler meantime when the TPS61194 power on , TPS61194'S input voltage is 5.2V, output setting is 9.9V as panel's spec. PWM pin shorted to VDDIO/EN Pin.
customer wants to know if the TPS61194 is not suitable to drive the 4S13P panel, as the reference schematic is for 4P8S Pannel application ,tks.