Other Parts Discussed in Thread: LMR36015-Q1
Hi,
i'm looking into potential replacements of LM25085 which not necessarily have to be pin-to-pin as we're working closely with customer on a tight BOM cost project. Here are some of the specs i'll require from the potential device.
- Vin max 42V, typ~15V. Vout 9V, 1A.
- device with better cost merit than LM25085
- additional information: ext FET or internal FET devices are good to go.
Regards,
Leo