Other Parts Discussed in Thread: PMP8740,
Hi,
I was trying to develop PMP8740 2KW full bridge dc-dc converter. But currently, bypassing the control card used by TI.
I have completed the power section and it is working well with external PWM signals.
Now I want to run it with UCC28950 on the board. But when I am trying to turn it on it is not producing any gate pulses.(the Current transformer is not attached, means ct+ and ct- are kept open )
I have checked the basic condition to turn on.
Vdd pin voltage > UVLO
SS/EN capacitor voltage >0.55 V(around 4.5V is coming)
The 5V ref is available and temp <140 degrees.
still, it is not producing pulses.
So what are the minimal requirements to turn it on(tested with no load)?
whether CT is mandatory to turn it on?
Regards.
Nidheesh.