This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: Replacement capacitor for unavailable values

Part Number: BQ76940


Good day,

In http://www.ti.com/lit/df/tidr773/tidr773.pdf, C24, C25, and C26 have values of 4700pF. If these capacitor values are unavailable, what capacitor value is suitable to replace those?

  • Hi Robert,

    The small capacitors on the TS pins are for slowing the edge rate since these pins are switched. However, these are not required. You can search for the closest value available. If these are not going to connect to a thermistor, it might be best to have no cap.

    Best regards,
    Matt