Part Number: LMG3411R050
Other Parts Discussed in Thread: LMG1210
Hi,
I was going through the article that was written on ti website about using a single pwm to control two GaN fets in a half bridge configuration with dead time here .
I also read that when using RC timed systems, we have to be careful about the degradation of capacitance over temperature and time. here
My application is in a home appliance that will go into widespread production. Even though temperature based degradation is not a concern for me (That being said, the temperature of the system can rise up to 60 deg C inside .).
But, I am wondering if aging due to time can, in fact, cause failures due to a gradual degradation of dead time and eventual shoot through events.
My questions are these to summarize :
How badly does aging due to time affect ceramic capacitors and should i be concerned while designing this board?
Are there any other reliable ways to have a complementary PWM with a single input?
How have the Ti Eval boards done so far in this setup so far?
Regards,
Tony