This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: Output overshoot

Part Number: TPS5430


Dear Team,

My customer is trying to build a design with TPS5430 to supply a pulsed load (actually a GPRS modem) which can draw up to 2A from almost no current levels. I have checked the schematics and it is looking OK. Layout is not perfect, but looks good.

According to Webench simulation, output voltage overshoot should be a little higher then 3.9V when the output voltage is set to 3.8V, but the customer sees overshoot exceeding 4.2V. Inductor value is 33uH and cap is 220uF electrolityc. I was not able to reach out the datasheet to see ESR. Tantalum caps are recommended on the datasheet. Could a standard electrolytic cap with high ESR cause such a big overshoot?

I can send the schematics and layout via email if needed.

Best Regards,

Caglar