This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196: Definition of 'Iout'

Part Number: TPS61196

I find some 'Iout' on the calculation formula of datasheet.
I use two pieces of TPS61196.
And I will flow 12string of LED by using 'multi-chip operation in parallel (Figure22.)'.
What value is IOUT when I flow 100mA per 1string? (1200mA? 600mA?)