This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: Need help in Configuring the gauge parameters

Part Number: BQ34110
Other Parts Discussed in Thread: EV2400, BQSTUDIO

Hi Team TI,

We have developed a custom board with BQ34110 fuel gauge IC. We are using LiFePO4 12.8V, 5.2Ah battery. I'm able to communicate with the IC and read Voltage, current, etc., We are majorly interested in SOC and SOH but we understood that we are reading other parameters with respect to default settings and need to change the chemistry and capacity related registers. To do this we need help in configuration of the Gauge parameters(Like Design Capacity, FCC, EDV0 Threshold and few other parameters).

We have read forum posts where they have been suggested to use EVM2300/EVM2400 USB-I2C modules. However, due to some constraints, we may not buy this anytime soon.

So my question is,

Without EVM2300/EVM2400 how do we configure the BQ34110 IC with above mentioned parameters.?