This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2372: 12.5k Phihong detection

Part Number: TPS2372

Hi All,

I'm developing a PD with the TPS2372 and I have a doubt about Phihong 12.5K detection resistor. When a Phihong injector detects a 12.5k resistor, it delivers power through the 4 pairs, but it still does classification?.

When my PD is configured to be used by an IEEE802.3bt PSE it is set  as Class 6 ( 24.9k detection) but when it is set to 12.5k detection resistor should it be set as class 4 or class 6?, or it is irrelevant as CLSA is 63.4ohm for Class 4 and Class 6 anyway?.  I have a switch to change from 24.9K detection to 12.5k and I don't know if I should use to change from 24.9k and Class 6 to 12.5k and Class 4.

Thanks,

Winsu