This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74801: Add a 2.2 Ohm to 5V on bias pin

Part Number: TPS74801


Hi, team

My customer have a application like the picture below, which add a 2.2 ohm resistor pull up to 5V.

Does this have a concern ? 

From the datasheet, " BIAS pin current's " current limit is 2mA. 

Does this resistor should be at least 5.1k ohm to fit the Bias pin current?