Other Parts Discussed in Thread: BQ27220, BQ4050, BQ34110
I have run the chem id test according to the directions several times with an EVE 105 AH cell. The results of one of the test follow:
Best chemical ID : 435 Best chemical ID max. deviation, % : 13.69
Summary of all IDs with max. DOD deviation below 15%
Chem ID max DOD error, % Max R deviation, ratio
435 13.69 0.9
446 14.42 0.08
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.
I am used to seeing deviation in the 7-8% range when I was testing a CALB 40 AH cell. Those tests also returned around 15 chem ids, not just two.
How should I interpret these results?