Hello,
We currently use the bq40z50-r1 in one of our batteries. About 10% of fresh new batteries are experiencing an OC condition. It seems that the OC condition only occurs during the very first charge cycle (at 99% SOC) and never appears after that. Our OC settings are as follows:
Threshold: 200mAh
Recovery: 2mAh
RSOC Recovery: 90%
RSOCL is set
The conditions for an OC flag to set are as follows:
RemainingCapacity() ≥ FullChargeCapacity() AND Internal charge counter ≥ OC:Threshold
We are not able to find much information regarding the internal charge counter. Does this counter begin once RemainingCapacity == FullChargeCapacity? When does the counter reset?
Thanks,
Edgar