Part Number: LM3644
hello
we want to set LM3644 in Flash mode, how do i to set the hardware and Registers?
Now out setting is:
1. TX pin was pulled down to Ground with 300K Resistor.
2. HWEN pin was pulled up to VDD.
3. STROBE pin connect with GPIO
After we write the register 0x01 to 0x8D, is it turn on the flash mode ? and do we need to send a high level interrupt to active Flash?
Now we write the register 0x01 to value of 0x8D, then read it, the value is 0x81; while we write to 0x8C, and read the value ,it become to 0x80.LM3644--SMV135A PC BOARD-A.pdf