Other Parts Discussed in Thread: TPS2663, TPS2660, TPS2120
Dear TI engineer.
I have questions about using the Or-ing system.
1) What are the functional differences other than the electrical characteristics of the LM74700-Q1 and LM5050-Q1?
If you choose one of the above devices and use the enable pin with Or-ing to get one power source.
2) Using one control signal, input the enable pin. Is there a problem if you connect the single inverter to one of the enable pins?
- I'd like to ask if there is a way to implement it in one control pin.
3) One of the two becomes enable off. Isn't this the power supply through the body diode of the FET?
- If it's powered at the same time, is there a way to deliver only one power source?
Thanks.