Hi,
I was following shortcuts indeed, As i was trying multiple modules for a better power management IC, I'm trying this BQ24650 MPPT charger IC, I need the Resistor Values that are to be fixed for the below requirements, I'm aware that the information is being given in the datasheet but it will be a hectic task for me to find.
Vmax(Solar Power) : 6V
Voc=12V
Imax:0.5 A
Pmax:3W
Need to charge a 3000mAH Li+ Battery
What are the Component values that i need to Fix,as in the Page no.22 in the datasheet of the application circuit of this module?
I have tried to fetch the design details using WEBENCH Power designer, but it did'nt displayed any designs for the above inputs.