Part Number: TPS22810
Hi, TI expert
Could you recommend me a power switch?
I need output delay time for 300~500ms.
Input: 12V, Output: 12V/3Amax
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mason,
Thanks for reaching out on E2E!
Please refer to our app note, Timing of Load Switches. You can increase the tdelay + trise time by using the TPS22810 with an extremely large CT capacitor. Since there is no limitation on the maximum value you can choose, a large CT capacitor will extend the tdelay + trise.
If you are looking to just change the tdelay time, you can try putting an RC delay on the enable pin. However, this will also increase your toff time.
Thanks,
Arthur Huang
To find the latest information on Power Switches, visit www.ti.com/powerswitch
Please click "This resolved my issue" button if this post answers your question.