This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65311-Q1: ADAS 4 IN 1 power management IC receommendation

Part Number: TPS65311-Q1
Other Parts Discussed in Thread: TPS62160-Q1, TPS65000-Q1

Hi team, 

For this specific requirement in camera ADAS system, 4 in 1 PMIC devices recommendation, TPS65311-Q1 is 8*8 package. Is there any other smaller size (like 3*3) recommentdation? 

DC-DC 8-12V     TO  3.3V           Max 500mA

       DC-DC              1.8V           Max 250mA   

        DC-DC/LDO     1.1V           Max 250mA

        LDO                 2.9V           Max 200mA

Best Regards,

Gene