This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256301: Chinese mean about datasheet

Part Number: UCC256301

What's the chinese mean of  " While designing for 150 W, take care in dimensioning the resonant tank components such that the system does not enter into the capacitive region of operation at 240 W", thanks!

  • Hi,

    I was unable to find this phrase in the English datasheet but I believe the point being made is to design the power stage so that in overload condition, the power stage has enough gain to avoid going into the capacitive region of operation. It is important to avoid the capacitive region because hard switching is induced on the primary MOSFETs and the control law inverts.

    Best Regards,
    Ben Lough