This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22917: reverse current protection

Part Number: TPS22917


Hi Experts,

I have a question about reverse current protection. The datasheet stated threshold current, 500mA(typ). If reverse current does not exceed IRCB how RCB will work? (For instance, IRCB is 200mA.)

Best Regards,
Fujiwara

  • Hi Fujiwara-san, 

    Thanks for reaching out on E2E!

    RCB activation current is the amount of reverse current required across the device when it is on to enable the reverse current blocking and turn the FET off. The device is looking for a voltage drop from VOUT to VIN so that RCB can be enabled. When the device is on, it takes that amount of current across the on-resistance of the device to cause that voltage drop.

    VIN leakage current is the current that leaks across to VIN when RCB is active.

    Thanks,

    Arthur Huang


    To find the latest information on Power Switches, visit www.ti.com/powerswitch

    Please click "This resolved my issue" button if this post answers your question.