Other Parts Discussed in Thread: IPG-UI,
Hello team,
One of my Customers is using TPS65086401RSKT in their project. They have given vsys 12V and shorted DRV5V_2_A1 and DRV5V_1_6 with LDO5P0 but not seeing proper output of this device. they have followed below sequence:
- CTL1 asserted.
- Buck 2 enabled (through I2C register).
- Buck 1 enabled after 2ms (through I2C register).
- Check the PG of Buck 2 and 1 on GPO1.
- Buck 5 enabled (through I2C register).
- Check the PG of Buck 2 and 1, and 5 on GPO2.
- LDOA2 enabled (through I2C register).
- Check the PG of Buck 2 and 1, and 5 and LDOA2 on GPO3.
- Buck 6 enabled (through I2C register).
- Check the PG of Buck 2 and 1, and 5 and LDOA2 and Buck 6 on GPO4
and measure below voltage on Input pins:
LDO5P0 : 5.027V
VSYS : 12.35V
LDO3P3 : 3.299V
VREF : 1.249V
DRV5V_2_A1 : 5.027V
DRV5V_1_6 : 5.027V
but getting below output:
BUCK1 : No output
BUCK2 : Output we are getting 0.88V
BUCK3 : NOT USED
BUCK4 : NOT USED
BUCK5 : No output
BUCK6 : No output
LDOA2 : Output we are getting 1.0V
They have also done below I2C setting:
- to set the required VID on all the VRs used (Buck 1, 2, 5 and 6 and LDOA2).
- enabled through I2C .
- configuring GPIOs for the Power Goods.
Please help me in resolving their issue..
Regards,
Vikas Chola