Other Parts Discussed in Thread: LM5170
Hello.
I am using the LM5170 to control a 4-phase buck converter. The buck is 48V/36V 1 kW. The controller is regulating the output voltage and it is able to handle transients, but I am having issues currently with current sharing among the four phases. My phase 1 and 2 share one controller and my phase 3 and 4 share another controller. Current is balance between phases 1 and 2 and current is balanced between phases 3 and 4, but the current balance is not balanced between the controllers. Phases 1 and 2 have way more current in them than phases 3 and 4.
I am using 1 voltage loop to set the ISETA pin for all four phases. I was wondering if I should be using 2 separate voltage loops, one for each controller? I do not know if the references are slightly off in the controller and if it is causing a large discrepancy between both controllers.