This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: how to choose a inductor value for buck charger of CC/CV

Part Number: LM5117

Hello:

Anyone can help me on how to choose a inductor value for charger using buck converter with CC/CV mode? I know for normal buck DCDC converter, the inductor is based on output current ripple/ switching frequency/ input , output ratio (Duty cycle). but for a charger using buck converter, how about during CC mode, the Vout is not fix value? or I  can calculate the L base on CV mode input/out ratio and ignore the CC mode condition

Such as if I want to use LM5117 to do a CC/CV mode charger with Vin=65V, Vout=56V (during CV mode) and Iout=2A(during CC mode). 

Thanks and Best Regards

Tong