Other Parts Discussed in Thread: TPS65400
Hi Team,
Would you advise that do you have power ICs such like TPS568215 which
has USB interface to control?
If no, are there any recommend circuit like reference design?
Thanks
Best regards,
Shidara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hao-san
Thank you very much for your support.
My customer is looking for the convienient device to control below items through USB,
Regarding to your inquiry, the customer is thinking below
1. VIN range : 11V to 13V
2. Vout : 0.8V to 5.5V
3. Max loading current : 6A
4. Do you just want to adjust the Vout voltage via PM Bus, or you need more functions? : more functions above.
Any advice should be highly appreciated.
Thanks
Best regards,
Shidara