This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5452: Isolated Gate Drive Design.

Part Number: ISO5452

Hello friends,

I am planning to use the isolated gate driver - ISO5452 in our gate driver design circuit. I wanted to know the conditions on pins namely - OUTH. I am planning to use IN+ and IN- will be connected to digital ground.

The conditions on rest of the pins is as follows:-

1) RST and RDY pins are high. 

2) IN+ is connected to GPIO with no input, mean to say it is floating. IN- is not used and connected to digital ground.

What will be the output on OUTH and OUTL pins with the above given conditions?