This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61181A: LED Driver

Part Number: TPS61181A
Other Parts Discussed in Thread: TPS60255, TPS54201

Hi,

I am using TPS61181A driver for driving 6 LED string in parallel (1 LED in each string) with IF = 20mA in each string and VF = 3.3V.

The input supply voltage is 19V and the required output is 3.3V.

Whether the driver supports the output of 3.3V?

If the driver is enough to support 3.3V, what will be the output voltage for sort circuit condition, single string open condition and entire strings open condition?

Please find the attached snippet for your reference

Kindly provide the required information.

Thanks.