Is there anything that can be considered as the cause?
AverageCurrent() 0x10 and 0x11 |
Voltage of Sense Resistor (0.01Ω) |
Current at current probe | ||
HEX | DEC | |||
- | (mA) | (mV) | (mA) | |
Charge | 359 | 857 | 5.990 | 610 |
Discharge | ffd3 | 45 | 0.338 | 33 |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AverageCurrent() 0x10 and 0x11 |
Voltage of Sense Resistor (0.01Ω) |
Current at current probe | ||
HEX | DEC | |||
- | (mA) | (mV) | (mA) | |
Charge | 359 | 857 | 5.990 | 610 |
Discharge | ffd3 | 45 | 0.338 | 33 |
Onyx -san,
Could you please let me know about below for this phenomenon?
1. As Chiaki -san explained, bq27426 value and measured value at sense register has large gap.
Charge : 857mA (bq27426) VS. 610mA ( measured value)
Discharge : 45mA (bq27426) VS. 33mA (measuerd value)
Will the gap be disapper if he run calibration? He afraid there is other facter for the gap because the gap is so large.
Could you pleae give your advice?
2. bq27426 isn't listed in the slua640 and Datasheet and TRM doesn't explain Host require Calibration.
Is the host calibaration required for bq27426,too?
Regards,
Nagata.