Other Parts Discussed in Thread: TPS650861, IPG-UI, BOOSTXL-TPS650861
hello:
I have bought two TPS650860EVM-116,I have two problems. 1:how can i change the buck2 step size from 25-mV to 10-mV, I want the buck2 voltage from default 3.3v to 0.8v(if used 25-mV step size,i used IPGUI only output 1V ) 2: i can change the voltage by the software IPGUI during the power on, but i will lose the change voltage if it power off and power on again .how could i save the change if i want the change voltage output again after i power down and power on?
thank you,dear!