This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050EVM-561: Capacity correction

Part Number: BQ4050EVM-561
Other Parts Discussed in Thread: GPCCEDV

Hello,

I'm using the bq4050-evm and according to the Technical Reference manual , the  FullChargeCapacity (FCC) updates after the battery undergoes a qualified discharge from nearly full to a low battery level and equals to:

FCC(new) = DCR (final) = DCR (initial) + Measured Discharge to EDV2 + (FCCx Battery Low%)
  
How do I set the low boundary Discharge voltage (EDV2) for Capacity Correcton in order to get a qualified discharge and do not force a Charging Operation immediately when reaching this threshold.
In addition, can you suggest a better method to correct the capacity errors caused due to finite resolution of the Coulomb counter?

Thank you for your help.