This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: status 0x0E, should it be changed to 02?

Expert 6460 points
Part Number: BQ28Z610

Hello,

We have update status=0x0E -> I assume we can create the golden file?

Is the below part of SLUA777 page 6 only about older devices, and not about bq28z610? 

„On legacy IT gauges, update status should be changed in the gg file from either 0E or 06 to 02 and once
the golden file has been programmed, IT enable command should be sent to turn on the algorithm. When
the IT enable command is sent, update status goes from 02 to 06. The reason for doing this is that
enabling IT also enables lifetime data. On this gauge, there is a separate command for enabling lifetime
data so Update status can be left as 06 for a 1s configuration or 0E for a 2s configuration.”


Another question, is it possible to use and store custom values in Serial Number and Manufacture Date in DF?
By default these are 1 and 0.

Thanks