Part Number: TLC59581
Dear experts,
I am designing LED display module using TLC59581. I would like to interface it with receiver cards. I noticed that the standard output or most common output of receiver card is HUB75 and it outputs 3 parallel data R G and B. I also noticed that in standard LED display module, it follows the receiver card providing parallel data input for R G and B. However, in TLC59581 the driver receives data through serial or SPI. Does this mean that an additional shift register is needed to convert the parallel input of R G and B to a single serial data input ? Thank you and looking forward to your reply.
Regards,
Reno