Other Parts Discussed in Thread: TIDA-01556
Hi,
I was very curious to know that the input voltage supply fed to the BQ25895 IC using various USB Sources, i want to know,like how the internal Mechanism detects if I feed the input power through USB using a Wall-Adapter,What settings it will take?
And Also, If I dont use a Standard USB based Charger, the input current Limit will be set to 0.5A. As mentioned in Datasheet
Page 17.
I will charge through a SOlar panel whose Imax would be 1.5A, what is the settings that I need to do for 1.5A input current.