Hello
1. Internal LDO
Could you tell me how muc efficency imporve if the internal LDO is used?
Best regards,
Tetsuro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
1. Internal LDO
Could you tell me how muc efficency imporve if the internal LDO is used?
Best regards,
Tetsuro
Hi Tetsuro,
Powering the internal LDO through the external BIAS_SEL pin will increase the efficiency as much as a couple of percentage points. It will all come down to what your operating conditions are.
Can you provide me with the following info: What is your input voltage, output voltage and output current? Are you tying your BIAS_SEL to Vout or an external power source? If an external power source, then what is the voltage?
Regards,
Alejandro
Tetsuro,
The image attached below demonstrates typical bench test data from an EVM for your application conditions. At a max load (4A) there is about a 1% efficiency increase when BIAS_SEL is connected to an external power source. Notice that at lower loads applying an external power source to BIAS_SEL can increase efficiency about 3%.
Regards,
Alejandro