Other Parts Discussed in Thread: BQSTUDIO
I have tried to follow the example from SLUUBD4.pdf, section 6.1, but I can not get the device to enter the FULL ACCESS mode.
Ideas / assistance ?
Time I2C command Comment
3.325841500000000, Write [0xAA] + ACK : UNSEAL part #1
3.325865000000000, 0x00 + ACK
3.325996000000000, 0x14 + ACK
3.326173500000000, 0x04 + ACK
3.331436000000000, Write [0xAA] + ACK : UNSEAL part #2
3.331459500000000, 0x00 + ACK
3.331591000000000, 0x72 + ACK
3.331768500000000, 0x36 + ACK
3.345636000000000, Write [0xAA] + ACK : Read status register on SEAL status (4) SEC1 and SEC0
3.345659500000000, 0x3A + ACK
3.345793500000000, Read [0xAB] + ACK
3.346244500000000, 0xA4 + NAK : <- Device is UNSEALED
3.346286500000000, Write [0xAA] + ACK : Request FULL ACCESS part #1
3.346309500000000, 0x00 + ACK
3.346660500000000, 0xFF + ACK
3.346839500000000, 0xFF + ACK
3.352099000000000, Write [0xAA] + ACK : Request FULL ACCESS part #2
3.352122500000000, 0x00 + ACK
3.352253500000000, 0xFF + ACK
3.352431500000000, 0xFF + ACK
3.455631000000000, Write [0xAA] + ACK : Read status register on FULL ACCESS status (2) SEC1 and SEC0
3.455654500000000, 0x3A + ACK
3.455788500000000, Read [0xAB] + ACK
3.456239500000000, 0xA4 + NAK : <- Device is still UNSEALED. Time 3.456 sec
3.555667000000000, Write [0xAA] + ACK
3.555690000000000, 0x3A + ACK
3.555824500000000, Read [0xAB] + ACK
3.556276000000000, 0xA4 + NAK
...
4.455817000000000, Write [0xAA] + ACK
4.455840500000000, 0x3A + ACK
4.455974500000000, Read [0xAB] + ACK
4.456426500000000, 0xA4 + NAK : <- Device is still UNSEALED. Time 4.456 sec (1 sec after)
4.555873500000000, Write [0xAA] + ACK
4.555897000000000, 0x3A + ACK
4.556031500000000, Read [0xAB] + ACK
4.556483000000000, 0xA4 + NAK
4.655838500000000, Write [0xAA] + ACK
4.655862000000000, 0x3A + ACK
4.655996000000000, Read [0xAB] + ACK
4.656448000000000, 0xA4 + NAK
4.755901500000000, Write [0xAA] + ACK
4.755925000000000, 0x3A + ACK
4.756059000000000, Read [0xAB] + ACK
4.756512000000000, 0xA4 + NAK
4.973305000000000, Write [0xAA] + ACK
4.973328500000000, 0x3A + ACK
4.973463000000000, Read [0xAB] + ACK
4.973914500000000, 0xA4 + NAK : <- Device is still only UNSEALED. Time 4.973 sec (1.5 sec after)
5.065832000000000, Write [0xAA] + ACK : Try to reset device - has no effect since device is not in full access.
5.065855500000000, 0x00 + ACK
5.065987500000000, 0x41 + ACK
5.066166000000000, 0x00 + ACK
Repeat sequence
5.165793500000000, Write [0xAA] + ACK : UNSEAL part #1
5.165817000000000, 0x00 + ACK
5.165948000000000, 0x14 + ACK
5.166125000000000, 0x04 + ACK
...