could you please suggest , how can i place lmg1020 in board...
i have a bga proto place machine but minimum size of bga component which can be placed is 5*5(mm) only...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
could you please suggest , how can i place lmg1020 in board...
i have a bga proto place machine but minimum size of bga component which can be placed is 5*5(mm) only...
Hi Hitesh,
After asking my team SMT, with out the proper pick and place machine the best way to solder the part is to place it by hand. Typically we pre-heat under the board and use a hot air gun on low airflow focused at the part on the top. Use solder paste and flux so that during reflow the part will self align and make solid connections on all 6 balls. Please let me know if this helps to answer your question or you have any more questions.
thanks,