Other Parts Discussed in Thread: TPS65310A-Q1
Hi ,
just want to check the main difference between TPS65311-Q1 and TPS65310-Q1? Thanks.
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
just want to check the main difference between TPS65311-Q1 and TPS65310-Q1? Thanks.
BRs
Given
Hi Given,
The product expert is on business travel, but I will take the first response while he is out, if there are additional details he can add them when he is available. The main difference between the TPS65311-Q1 and the TPS65310A-Q1 is the switching frequency for the DCDC converters.
|
TPS65310A-Q1 |
TPS65311-Q1 |
Synchronous-Buck Controller |
490 kHz |
490 kHz |
Dual-Synchronous Buck Converter |
0.98 MHz |
2.45 MHz |
Adjustable Asynchronous-Boost Converter |
0.98 MHz |
2.45 MHz |