I added a gauge chip to my existing charger design. I asked a question here, but was asked to re-post to get someone from the charger team to look at it. I have most of the design in the charger worked out. Can someone help with the following questions:
- There is a 10uF cap(c28) across the pack terminals (from the BQ24032A design). Now that the gauge output is connected to the BAT terminal of BQ24032A chip, do I keep the cap?
- Can the CE chip on BQ24032 be pulled up with a 10k resistor or needs some other valued resistor (since PSEL has 100k pull-up). I want ACIN to be connected to out in the absence of BAT input.
- Can the LDO pin on BQ24032 be left unconnected?