I have a design that uses the BQ27441DR as a battery metering unit.
I have built several of these units and at the beginning they seems to be working well, but just recently I have built few more boards and none of them work.
Same design same firmware, no changes whatsoever on the design, and nothing work (from the BQ27441) interface side. I did notice that the VDD pin-5 is always 0.025 Volts even though the battery voltage is 3.7 Volts. Is this a reason that the BQ27441 does not work? Is there a way to force the VDD to be on all the times. All the boards that work have a VDD of 1.8 Volts