Hi team
How do I handle unused pins in TPS2373-4?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Charles,
It is recommended to use TPx/BT signals as described in the FAQ below:
However, if for your application there is no use for it, you can leave TPx/BT pins OPEN.
For UVLO_SEL, it depends on the UVLO of the PWM controller you are pairing it with. If above 7.25V then it is recommended to leave it OPEN. If below 7.25V then it should be connected to RTN.