This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400: Fault condition

Part Number: TPS65400

Hi, team

Buck3 is not output.

The register is as follows. What is the cause?

 78h 0x01, 7Ah 0x10

Is IOUT_OC flag 1 if it detects OCP even once?

Best Regards,

  • Hi,

    These register values can't provide much information.
    Did you select PAGE=0x02 first?

    2. Yes, the flag will be kept there until you clear it manually.

    Regards,
    Hao
  • Hi, Hao.

    In the data sheet,

     During the soft-start time for a switcher, all fault signals (OVP, OCP, and UVP) are disabled and reset to the unfaulted condition. The first moment when faults can be triggered is after the end of the soft-start sequence.


    Is it correct that the OCP flag is not set during soft start?
    If at the end of soft start the output voltage has not reached the setting, does OCP and UVP simultaneously flag?
    If the output voltage drops due to Dmax constraints, does the UVP flag go on?

    Best Regards,

  • Hi,

    1. Yes, OCP flag is not set during soft start.
    2. OC flag and UV flag will be set immediately after soft start if there is OC/UV condition.
    3. UVP flag will be set up as long as Vout is under the UVP threshold, if it touched the Dmax contraints and still not in UVLO, UVP could go on.

    Regards,
    Hao