Other Parts Discussed in Thread: TINA-TI
Ok: seems what I am looking for is perhaps best obtained by "properly" using UCC28780.
I am trying to obtain max efficiency from flyback isolated converters with low powers ( I need 6 such). Input is regulated 380VDC. Outputs 5, 12 & 15 from .5 amp tp 6 amp.
This one has active clamp & recovers power to deliver to the output.
I find out that there are so many under the hood stuff one needs to explore before designing in as stand-alone modules for a larger system that simulation is a sure risk mitigating aspect when pressed in time & funds.
Is there any model in TINA-TI?
I see there is an eval module, do you suggest to work on that to find out all ifs-buts-what ifs?
thnx
-robin