This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Asking for the buck and boost converter recommendation

Other Parts Discussed in Thread: TPS62180, TPS54824

Hi Team,

Customer is looking buck and boost converter solutions.
Would you please recommend the proper solution for this?

Buck converter
Vin=15V, Vout=4V, Iout=6A

Need 2 phase, because we have maximum height limitation, need low down inductor current to reduce inductor size.

Or one phase solution but inductor can under 0.47uH.


Boost converter
Vin=7~8.8V, Vout=15V, Iout=2.5A. Also need support inductor value can under 1uH.

BR,
SHH