This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV716P: Is there a TLV716P with two output 3.3V?

Part Number: TLV716P

Dear Sir/Madam,

Can I check if I want to use TLV716P with input voltage 5V and both output regulator at 3.3V, which full TI part no should I use? 

can this be done? 

Based on the sample request part no, i did not find one something like TLV7163333PDPQR

Please help to clarify

Best Regards,

KPK

  • Hi KPK,

    While you are correct on what the part number would be, there is not a dual 3.3 V output version of TLV716P at this time. You can always find the available options in the Package Option Addendum which is appended to the end of the datasheet.

    Very Respectfully,
    Ryan