Hi,
I am using a BQ34z100-g1 with an 8s2p LiFePO4 batteries. I have one doubt about the realtion between quit current, charge current and discharge current.
We have a system with a permanent current consumption of 40mA. Each 2/3 hours the current consumption rise to 3-4A during 20-25s. The battery is always powering the device so the consumptions seing from the battery are the same.
The charge procedure of the battery force to sometimes charge it with 30mA during 10-20 minutes to balance its cells. In normal operation the charge current is 2A in CC and when in CV it drops to 80mA when we program the charge final.
Which values of quit current, charge current and discharge current should we program?
Thankyou,