Other Parts Discussed in Thread: LM5176
We make use of the LM5022 in a Sepic converter, in a 3 phase interleaved configuration, following TI's advice as stated below:
(1) Use one LM5022 as the Master, and the other as the slave, by tying the slave's FB pin to GND, and it COMP pin to the master's COMP pin;
(2) Provide an external clock to each LM5022 to synchronize their switching to avoid beat frequency.
(3) If you want to interleave operation, you should provide 180 degree phase shifted clock signals to each LM5022.
We provide 3 120 degree out of phase clocks. This works great.
Question: when the COMP pins are tied together, and the FET of each branch has it's own current sense resistor to each controller, the currents are not always equal in each branch. We see up to 20% difference in voltage on each current sense resistor at the point where the FETs turn off per branch.
What is the tolerance in the relation between the COMP pin voltage and the current at which the FETs are turned OFF. From the internal block diagram of the control IC there are two diodes and a resistive divider in between. What is the accuracy and temperature effect here?
Robert