Other Parts Discussed in Thread: LM25017, LM5030, UC2844, UCC21530, TIDA-00174
Hi,
I am designing a phase shifted full bridge dc-dc converter.
Input voltage: 400VDC; Output voltage: 650VDC; Power: 3500W; Frequency: 200kHz.
Please provide power supply recommendations for UCC21520, used to gate each of the half bridge, preferably one power supply module that can provide 3 or 4 isolated voltages. Also, thoughts on how the design can be completed with minimum number of power supplies are highly welcome.
The board has a 24VDC bus.
Regards,
Lakshmi.