Hi
My customer use TPS56528.
They would like to decrease feed back resister value by single digit from recommending components value of table2.
Is this OK?
If there are an problems, could you tell me them?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer use TPS56528.
They would like to decrease feed back resister value by single digit from recommending components value of table2.
Is this OK?
If there are an problems, could you tell me them?
Hi Iven-san
Thank you for the reply and I'm sorry for my lack of explanation.
ex.When I set Vout at 1V, the recommending feed back resiter value is R1=33.2kΩ and R2=49.9kΩ in table 2.
In this case, could I select R1=3.32kΩ and R2=4.99kΩ?
Hi
My customer reduce the output ripple by decrease the feed back resister value.
And they could reduce the ripple by that's method.
Could I get the answer to the following questions?
-Decrease feed back resister value by single digit from recommending components value of table2
-Acceptable range to be able to decrease resister value
-Problems when I decreased resister value