Other Parts Discussed in Thread: BQSTUDIO,
Hello,
I was able to get through configurations with the BQ40Z80EVM-020, and I moved to our custom PCB. The circuitry is nearly an exact replica of the EVM circuitry with a few exceptions on the CHG FET drive circuit. We are not using a PRE-CHG or PRE-DSG circuit.
My question is, when we go through checkout is there a way to have to avoid having pack voltage connected? I have seen several postings () saying to keep the device communicating reliably we need to have PACK voltage connected. I have configured the device to not go into sleep mode, and I am using a *PRESENT pin to detect the pack is enabled. I have ensured that the pin is < 0.55V per the data sheet. It seems to me that this should be sufficient to bring the device on and start communicating with bqStudio. What is the reasoning behind requiring voltage at the PACK pin?
I have attached my configuration settings in case I am missing something.
Thanks,
Adam Drewery