Other Parts Discussed in Thread: UCC29002
Ulrich: Let me push it a bit on the application range of UCC28780 ( now that we have the EVM)- can these be put in parallel?
No just 1 but in our case, we would want either 3 in parallel or a multiple of them.
Think of the reason behind triplets & wide applications that open up.
BTW: it dawned on me out of the blue that I should use LGM3410 HB here!
What a wonderful idea....
And, a question: they say you have 2 options for ripple cancellation- passive & active.
Elsewhere, it seems to read like one needs both. Could you pl clarify?
In our mini pkg, every part addition counts. If we can get the same efficiency without some parts, we will chop them off...
thnx
robin